Back to:
Press Releases
Press Release Detail:
Thorlabs Releases New sCMOS Cameras
Newton, NJ – October 10, 2017–
Thorlabs has announced the release of its new 2.1 Megapixel Quantalux™ sCMOS Camera based on a high-performance 1e- read-noise imager. Ideal for demanding imaging applications, the monochrome sensor can image the full frame [1920 (H) x 1080 (V)] at 50 fps with 16 Bit resolution and offers a peak quantum efficiency of 61% at 600 nm. Packaged in a housing that measures just 2.38" (at its widest point) x 2.78", the sCMOS camera is equipped with passive thermal management for the sensor, reducing dark current without the need for a cooling fan or thermoelectric cooler. A USB 3.0 interface provides compatibility with most computers.
"We are excited to introduce Quantalux, a camera with superb 1e
-
read noise and high dynamic range. Our goal was to achieve a price/performance level that provides researchers and OEMs with a cost effective option for achieving low-light images without compromising on key specifications," commented Jason Mills, General Manager of Thorlabs Scientific Imaging. "In addition to the outstanding performance, Quantalux users can benefit from the ease of integration with a comprehensive software suite that includes ThorCam (our Windows GUI) as well as support for third-party applications such as ImageJ/Micromanager, LabVIEW
®
, MatLab
®
, and our developer-friendly SDK."
The compact housing of the Quantalux sCMOS camera is feature rich, enabling seamless integration into a multitude of setups. An adjustable C-Mount adapter is factory installed into the SM1-threaded optical aperture of the camera for out-of the-box compatibility with industry-standard microscopes and camera lenses. Various mounting taps are also provided for optical post and 30 mm cage system compatibility.
Suggested applications include fluorescence microscopy, VIS/NIR imaging, multispectral imaging, and low-light inspection. To see our full line of Scientific Cameras, please visit
thorlabs.com
.
About Thorlabs:
Thorlabs, a vertically integrated photonics products manufacturer, was founded in 1989 to serve the laser and electro-optics research market. As that market has spawned a multitude of technical innovations, Thorlabs has extended its core competencies in an effort to play an ever increasing role serving the Photonics Industry at the research end, as well as the industrial, life science, medical, and defense segments. The organization’s highly integrated and diverse manufacturing assets include semiconductor fabrication of laser diodes, optical amplifiers, lithium niobate modulators, quantum cacscade/interband cascade lasers, and VCSEL lasers; fiber towers for drawing both silica and fluoride glass optical fibers; MBE/MOCVD epitaxial wafer growth reactors; extensive glass and metal fabrication facilities; advanced thin film deposition capabilities; and optomechanical and optoelectronic shops.