| Motion Control SoftwareAn updated EEPROM in motion control stages sold starting in early 2022 necessitates a controller firmware upgrade. If you receive an "unknown stage" or "phasing error" message, please update your Kinesis software to the latest version, and use the firmware update utility available separately for download in the Utilities tab.Thorlabs offers two platforms to drive our wide range of motion controllers: our XA software package and our Kinesis software package, which is being phased out. The Kinesis software supports most of Thorlabs' motion control products. The XA software is an improved platform for developers that currently supports some of our most popular motion control products (see the full list of supported products here). Both the Kinesis and XA software packages feature .NET controls which can be used by 3rd party developers working in the latest C#, Visual Basic, LabVIEW, or any .NET compatible languages to create custom applications. Low-level DLL libraries are included for applications not expected to use the .NET framework, and APIs are included with each install. The Kinesis software includes a Central Sequence Manager that supports integration and synchronization of all Thorlabs motion control hardware and a simulator is included to assist in developing applications without requiring hardware. Guides to using our Kinesis software package with LabVIEW can be found here. XA developer guides, code examples, and API documentation can be found in the XA software development kit (SDK). Full API documentation for XA is provided for the native C library. The .NET wrapper documentation is currently under development. Please contact Tech Support for more details on using the .NET wrapper. Note: While select products are still capable of running the legacy APT™ software package, this platform is no longer fully supported. Information on software compatibility can be found in the product documentation, and additional details about the APT software can be found here.
 Kinesis Software: Kinesis software installation package.XA Software: XA software installation package.Firmware: Firmware Update UtilitiesCommunications Protocol: Document describing the communications commands for the Kinesis, XA, and APT software packages.GitHub Resources: Link to Thorlabs' motion control content on GitHub®.Support: Calibration tool for the PDXC2 controller.Archive: The previous versions of the software.APT Software: APT software installation package.
 
| Communications Protocol |  |  | 
|---|
 | Description | This is a .pdf file describing the communications commands for all APT-, Kinesis-, and XA-compatible devices. |  |  | Version | 42.1 |  | Filesize | 5.67 MB |  | Download |  
 Only download from trusted sources, like Thorlabs, and always scan files before executing. | 
| GitHub® Resources |  |  | 
|---|
 | Description | Thorlabs has been expanding our offering of example code for the Motion Control products on our GitHub account. These include examples for the C++, C#, MATLAB®, and Python programming languages, and are a useful starting point for implementing Thorlabs' devices in common applications. |  |  | Additional | Please click the icon below to visit our GitHub page. | 
| PDXC2 Calibration Tool |  |  | 
|---|
 | Description | This tool is used to recalibrate the PDXC2 controller with the PDX1 and PDXR1 ORIC piezo inertia stages with encoders. |  |  | Version | 1.1.0 |  | Filesize | 128 KB |  | Download |  
 Only download from trusted sources, like Thorlabs, and always scan files before executing. |  | Change Log |  | 
| PDXC2 Calibration Tool |  |  | 
|---|
 | Description | This tool is used to recalibrate the PDXC2 controller with the PDX1 and PDXR1 ORIC piezo inertia stages with encoders. |  |  | Version | 1.0.0 |  | Filesize | 130 KB |  | Download |  
 Only download from trusted sources, like Thorlabs, and always scan files before executing. |  |